Constant Temperature Control for the High-Precision Electronics of Particle Accelerators
With the Varistar LHX+ air-water heat exchanger, nVent SCHROFF has developed a market-ready, standardized modular cooling system for technologically advanced test and measurement applications. It was developed for...
Our Latest Stories


Critical Factors to Consider in a Modular COM Express System Build
Small form factor solutions such as COM Express (Computer On Module) are becoming ever more popular, able to solve problems that used to be approached using modular 19”…