How nVent ERIFLEX’s Safe, Reliable, Space-Saving and Time-Saving Products Can Benefit Specifying Engineers and Contractors
nVent ERIFLEX provides low-voltage connection and distribution products for several applications, including, but not limited to energy storage systems, fast DC chargers, battery packs, inverters, transformers, combiner boxes,...
Our Latest Stories


How nVent Renewable Energy Solutions Contribute to a Safe and Sustainable World
Renewable energy is an increasingly popular source of power. Renewable energy sources will continue to sit at the forefront of the push for sustainable practices in the modern…


nVent ERICO Supports Utilities with Compatibility with Copperweld to Bring Reliable, High-Performing Utility Grounding and Bonding Connection and Conductor Solutions to the Grid
nVent ERICO and Copperweld® now offer compatible grounding and bonding connectors and conductors for the utility market. With the demand on the power grid increasing daily, it’s vital…


Utility Case Study: Energy Transmission Line Application in Denver, Colorado
CHALLENGE A new energy transmission line was installed requiring 5500 square feet of ground mesh for proper grounding and bonding of the high-voltage lines and towers. It also…


Utility Case Study: Substation and Transmission Project in Big Bear, California
CHALLENGE Several challenges were identified in the construction of a new 20/115 kV substation, along with adding the associated telecommunications and distribution lines.They also needed to replace a…


Utility Case Study: Substation Application in Columbia, South Carolina
PROJECT TYPE Utility required appropriate grounding for a new substation including equipotential safety comprised of 4/0 ground grid at 24″ below grade was supplemented by a custom-made nVent…


Why the nVent ERICO Hammerlock Ground Clamp Simplifies Installation and is the Reliable Choice for Power Utility Distribution
With the demand on the power grid increasing daily, it’s vital to have reliable products throughout power infrastructure. In addition, updating current infrastructure is essential to handling disruptions…


Energy Storage and E-mobility from nVent Electrical Solutions
nVent is the leading provider of grounding, bonding and power connection solutions for energy storage applications compliant with UL 9540 or the IEC 62933 series of standards. Demand…


Build a Better and More Resilient Power Grid
Updating and equipping the power grid and existing infrastructure to handle disruptions and avoid outages is a key issue all utilities are facing and will continue to face…


Grounding Myths: Part 4 – Electrical Safety
In the final blog post of nVent ERICO’s four-part blog series addressing the common myths and misconceptions which create confusion around the design and installation of grounding systems,…


Grounding Myths: Part 3 – Association of the Diameter of Ground Rods and Ground Resistance
In the first two posts, we hit on a few very common myths when it comes to grounding including which product type will perform the longest. In the…