How nVent ERIFLEX’s Safe, Reliable, Space-Saving and Time-Saving Products Can Benefit Specifying Engineers and Contractors
nVent ERIFLEX provides low-voltage connection and distribution products for several applications, including, but not limited to energy storage systems, fast DC chargers, battery packs, inverters, transformers, combiner boxes,...
Our Latest Stories


How Transient Discriminating (TD) Technology Improves Surge Protective Device (SPD) Life and Safety
Surge protection is a fundamental requirement for safeguarding a facility against electrical events. Specifically, a surge protective device (SPD) is designed to limit transient voltages and divert surge…


7 Electrical Engineering Marvels We Could Not Live Without [Plus Practical NEC Tips]
Electrical engineering is a complex field that makes life easier for us all. In this post, we will first overview seven of those electrical engineering wonders that accelerated…


IEEE 837 Explained: How Permanent Grounding Connections Are Qualified
When electrical professionals install grounding systems, they need to have confidence that the design and installation will assure protection reliably for the expected life of the system. Grounding…


A Basic Overview of Exothermically Welded Connections
When constructing electrical protection systems, electrical grounding connections must remain dependable over the life of the system. If bonds weaken, grounding, bonding and lightning protection systems become susceptible…


5 Ways to Prepare a Home’s Surge Protection for Storm Season [Plus More Electrical Engineering Information]
In this edition of electrical engineering industry news, see what electrical professionals can do to get their clients prepped for storm season, what the National Electrical Code (NEC)…


Happy Birthday to Us, Thanks to You!
Readers – Thank you for making the first year of the nVent ERICO blog a success! We have enjoyed bringing you information about grounding, bonding, lightning and surge…


Telecom Equipment Near Electrical Transformers: 6 Scenarios That Require Extra Care
This following is part of our telecom lightning protection series, which is based on our whitepaper “Earth Potential Rise in Public Spaces Near Telecommunications Facilities,” that was published…


Fewer OSHA Inspections May Mean Increased Risk [and Other Electrical Industry News]
The Occupational Safety and Health Administration (OSHA) is running a leaner, tighter ship these days, with a continued, aggressive approach to enforcement and an increase in the cost for violations…


3 Lightning-Related Problems for Telecommunication Towers in Very Dense Cities
This following is part of our telecom lightning protection series, which is based on our whitepaper “Earth Potential Rise in Public Spaces Near Telecommunications Facilities,” that was published…


What Are the Basic Differences Between UL 96A, NFPA 780 and LPI 175?
For electrical engineers, contractors, installers, designers and other individuals whose jobs involve lightning protection systems and related equipment, understanding all the relevant standards can be a daunting task….