nVent is Your Partner in Rapid Power Restoration
Recover from the Disaster Faster When disaster strikes and power outages occur, utility companies face immense pressure to restore electricity swiftly and efficiently. Utilco (now part of nVent)…


Recover from the Disaster Faster When disaster strikes and power outages occur, utility companies face immense pressure to restore electricity swiftly and efficiently. Utilco (now part of nVent)…


nVent ERICO and Copperweld® now offer compatible grounding and bonding connectors and conductors for the utility market. With the demand on the power grid increasing daily, it’s vital…


CHALLENGE A new energy transmission line was installed requiring 5500 square feet of ground mesh for proper grounding and bonding of the high-voltage lines and towers. It also…


CHALLENGE Several challenges were identified in the construction of a new 20/115 kV substation, along with adding the associated telecommunications and distribution lines.They also needed to replace a…


CHALLENGE Existing transmission lines from the 1960’s needed to be replaced in a “sugar sand” soil. The customer needed an efficient-to-install, theft-deterrent grounding solution that would achieve desired…


PROJECT TYPE Utility required appropriate grounding for a new substation including equipotential safety comprised of 4/0 ground grid at 24″ below grade was supplemented by a custom-made nVent…


As the demand for renewable energy sources continues to rise, utility-scale battery energy storage systems (BESS) have emerged as a crucial component in the quest for sustainable power….


nVent ERIFLEX provides low-voltage connection and distribution products for several applications, including, but not limited to energy storage systems, fast DC chargers, battery packs, inverters, transformers, combiner boxes,…


Renewable energy infrastructure demands stronger, more dependable electrical system connections to ensure safe and productive operations. The typical solar power array is designed for at least 30 years…


nVent provides a range of solutions for electrical panels that allow for greater design flexibility, including more ways to compress an electrical panel and overcome spatial limitations. nVent…