Select your Language Preference

nVent ERICO

Utility Case Study: Energy Transmission Line Application in Denver, Colorado

CHALLENGE A new energy transmission line was installed requiring 5500 square feet of ground mesh for proper grounding and bonding of the high-voltage lines and towers. It also…

Utility Case Study: Substation and Transmission Project in Big Bear, California

CHALLENGE Several challenges were identified in the construction of a new 20/115 kV substation, along with adding the associated telecommunications and distribution lines.They also needed to replace a…

Utility Case Study: Substation Application in Columbia, South Carolina

PROJECT TYPE Utility required appropriate grounding for a new substation including equipotential safety comprised of 4/0 ground grid at 24″ below grade was supplemented by a custom-made nVent…

Why the nVent ERICO Hammerlock Ground Clamp Simplifies Installation and is the Reliable Choice for Power Utility Distribution

With the demand on the power grid increasing daily, it’s vital to have reliable products throughout power infrastructure. In addition, updating current infrastructure is essential to handling disruptions…

Energy Storage and E-mobility from nVent Electrical Solutions

nVent is the leading provider of grounding, bonding and power connection solutions for energy storage applications compliant with UL 9540 or the IEC 62933 series of standards. Demand…

Power Utility Transmission Lines

Build a Better and More Resilient Power Grid

Updating and equipping the power grid and existing infrastructure to handle disruptions and avoid outages is a key issue all utilities are facing and will continue to face…

Grounding Myths: Part 4 – Electrical Safety

In the final blog post of nVent ERICO’s four-part blog series addressing the common myths and misconceptions which create confusion around the design and installation of grounding systems,…

Grounding Myths: Part 3 – Association of the Diameter of Ground Rods and Ground Resistance

In the first two posts, we hit on a few very common myths when it comes to grounding including which product type will perform the longest. In the…

Grounding Myths: Part 2 – Galvanized Rods vs. Copper-Bonded Rods

The second post in the nVent ERICO four-part blog series addressing the common myths and misconceptions which create confusion around the design and installation of grounding systems is…

Grounding Myths: Part 1 – Low Earth Resistivity, Earthing vs Grounding, Electrical Currents

nVent ERICO is launching a four-part blog series addressing the common myths and misconceptions which create confusion around the design and installation of grounding systems. Several of these…