Select your Language Preference

September 2018

News | Meet The Team | Tradeshows | Useful Links   News EC&M’s Product of the Year Platinum Award Goes to Angled Trough nVent’s HOFFMAN Angled Trough recently…

Four Ways Wire Rope is Better than Jack Chain

CHOOSING A SUPPORT SYSTEM: Wire rope support systems provide benefits to make them a superior support method compared with threaded rod, jack chain and metal strap. Discover the…

The Pros and Cons of 4 Common Ground Rod Materials

When it comes to selecting a ground rod, engineers must avoid a one-size-fits-all approach. Different factors—material, soil resistivity, location, facility type, size, among others—play into the overall efficiency…

Four Traits of Spring Steel That Makes it the Ideal Material for Fasteners

In 1956, the CADDY brand was the first to develop and market spring steel fasteners. Since then, spring steel has gained popularity, and the offering has expanded due…

For More Efficient Onboard Electrical Systems, nVent ERIFLEX Connections Make a Difference

  When it comes to transporting people and goods, railroads typically have a lower environmental impact than other modes of transportation. Further, many regions around the world are…

What Is the Difference Between Copper-Clad and Copper-Bonded Steel?

When discussing the components in an electrical grounding system, we often hear the terms “copper-clad steel” and “copper-bonded steel” used interchangeably.Though it may seem inconsequential, each term represents…