Select your Language Preference

Lightning_Fires.pngFrom 2007 to 2011, it’s estimated that U.S. fire departments responded to an average of 22,600 fires started by lightning per year. While humans cause more fires than lightning, studies show that the devastation of lightning-caused fires is significant. 

The harm of direct lightning strikes is widely known, but recognizing the prominence of fires caused by lightning is equally important to understand, as we can play a role in minimizing them. 

Continue reading to learn how lightning causes fires, and how you can protect your facility from the associated damage.

Lightning vs. Human-Caused Wildfires 

You can probably hear Smokey Bear saying it now: “Only you can prevent forest fires.” Believe it or not, that slogan started more than 60 years ago, and still has relevance today. Recent research shows, in fact, that humans cause 84% of all wildfires.

While that staggering number should put you on guard, an emphasis on fires caused by lightning strikes cannot be ignored. Lightning triggers about 14% of all reported wildfires, and these fires damage far more land than those caused by humans—an average of 500 acres per fire compared to 40 acres.

The Damage of Lightning-Caused Fires

Wildfires in open fields and forests across the Midwest and West Coast capture the news for their widespread devastation, but fires in the home may be your biggest concern. From 2004 through 2008, only 18% of lightning fires occurred in homes, but these accounted for 70% of the direct property damage, which equated to $407 million.

How Can Lightning-Induced Fires Be Prevented?

While fires caused by lightning strikes aren’t considered human-created, available technology can decrease the number of fire disasters caused by lightning.

Lightning protection systems require a systematic and comprehensive approach to minimizing threats caused by transients, which are the surges in voltage that occur from lightning strikes. The four-step protection process includes the following:

  1. Interception of the lightning flash through an air termination device.
  2. Conducting the lightning strike to the earth, which depends on a straight, seamless stream of conductors for the current to pass through.
  3. Dissipating the current into the earth and away from the facility.
  4. Creating an equipotential bond, which is required to eliminate voltage gradients and reduces the possibility of electric shock or electrical equipment fault.

Whether you are responsible for the protection of a residential home, facility or other entity, consider the role you play in protecting it from all lightning-related fires seriously.

>>>Related Read: 4 Components to Protect Residential Homes from Lightning Damage

For a more holistic look at lightning protection systems, check out this resource on six steps to more comprehensive lightning protection systems. 

As mentioned in the four-step protection process, interception of the lightning flash is the critical first step. Without effective air termination placement, the rest of the system will be ineffective in protecting the structure. A massive study of the Collection Volume Method (CVM) for lightning protection systems provides new understandings of air termination placement. Download your copy of the study today.

Image credit: Pixabay