Select your Language Preference

Three Ways CADDY SUPERFIX is Better than a Split Ring Hanger

A split ring hanger can effectively hold a pipe from a threaded rod, but if you donot have three hands, they can be very difficult to install. CADDY SUPERFIX is designed make installation much easier. Unlike a split ring hanger, CADDY SUPERFIX has the added benefits of:

  1. One-handed closing– The CADDY SUPERFIX locking device can be closed with just one hand, making it possible for one person to easily install a piece of pipe.
  2. Noise reduction– The rubber lining on the inside of the clamp holds the pipe firmly in place and can serve as noise reduction.
  3. No loose hardware– In the video, Rick makes it very clear that when using a split ring hanger, the installer should put the screw “somewhere where you can find it.” This is because the small loose screws can easily be dropped, lost, or misplaced. The screw in CADDY SUPERFIX does not need to be completely removed to open and close the clamp.

Fun Fact:  The “third hand” in this video was that of the Product Manager for CADDY SUPERFIX and many of our other products that serve the plumbing and HVAC markets.